Part Number: 66AK2E05
Hi,
It seems that it is not possible to build last version of Processor SDK Linux (06_03_00_106) for k2e platform anymore.
These steps from documentation (1.2. Building the SDK — Processor SDK Linux Documentation) are not possible since git://arago-project.org does not exist anymore:
$ git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk $ cd tisdk $ ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-<version>-config.txt $ cd build $ . conf/setenv $ export TOOLCHAIN_PATH_ARMV7=$HOME/gcc-arm-8.3-2019.03-x86_64-arm-linux-gnueabihf $ export TOOLCHAIN_PATH_ARMV8=$HOME/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu $ MACHINE=am57xx-evm bitbake arago-base-tisdk-image
I did not see any end of support of k2e platform on the website.
What is the situation with this SOC?
Best Regards