Part Number: TMS320C5535
Hi,
Customer calculates the 2048-point FFT according to the Greater Than 1024-point FFT code provided in the manual, the result of the FFT combination of odd-even sequences is wrong.
He uses the following CPLX_Mul code, the multiplication and shifting of two int16 numbers will cause the sign bit to be shifted to the right.
Int32 CPLX_Mul(Int32 op1, Int32 op2)
{
Int16 op1_r, op1_i, op2_r, op2_i;
Int32 op1_op2_r, op1_op2_i;
Int16 op1_op2_r16, op1_op2_i16;
Int32 cplx_prod;
// Mask data for real and imag data = (real:imag)
op1_r = op1 >> 16;
op1_i = op1 & 0x0000FFFF;
op2_r = op2 >> 16;
op2_i = op2 & 0x0000FFFF;
op1_op2_i = (Int32)op1_r*op2_i + (Int32)op1_i*op2_r;
op1_op2_r = (Int32)op1_r*op2_r - (Int32)op1_i*op2_i;
op1_op2_i16 = (Int16)(op1_op2_i >> 15);
op1_op2_r16 = (Int16)(op1_op2_r >> 15);
cplx_prod = (((Int32)op1_op2_r16 & 0x0000FFFF)<< 16);
cplx_prod = cplx_prod | ((Int32)op1_op2_i16 & 0x0000FFFF);
return cplx_prod;
}
Int32 CPLX_Add(Int32 op1, Int32 op2 , Uint16 scale_flag)
{
Int16 op1_r, op1_i, op2_r, op2_i;
Int32 op1_op2_r, op1_op2_i;
Int16 op1_op2_r16, op1_op2_i16;
Int32 cplx_prod;
// Mask data for real and imag data = (real:imag)
op1_r = op1 >> 16;
op1_i = op1 & 0x0000FFFF;
op2_r = op2 >> 16;
op2_i = op2 & 0x0000FFFF;
// Yr = 1/2 * (op1_r + op2_r), Yi = 1/2 *(op1_i + op2_i)
op1_op2_i = (Int32)op1_i +(Int32)op2_i;
op1_op2_r = (Int32)op1_r +(Int32)op2_r;
op1_op2_i16 = (Int16)(op1_op2_i >> 1);
op1_op2_r16 = (Int16)(op1_op2_r >> 1);
cplx_prod = (((Int32)op1_op2_r & 0x0000FFFF)<< 16);
cplx_prod = cplx_prod | ((Int32)op1_op2_i & 0x0000FFFF);
return cplx_prod;
}
Int32 CPLX_Subtract(Int32 op1, Int32 op2 , Uint16 scale_flag)
{
Int16 op1_r, op1_i, op2_r, op2_i;
Int32 op1_op2_r, op1_op2_i;
Int16 op1_op2_r16, op1_op2_i16;
Int32 cplx_prod;
// Mask data for real and imag data = (real:imag)
op1_r = op1 >> 16;
op1_i = op1 & 0x0000FFFF;
op2_r = op2 >> 16;
op2_i = op2 & 0x0000FFFF;
// Yr = 1/2 * (op1_r - op2_r), Yi = 1/2 *(op1_i - op2_i)
op1_op2_i = (Int32)op1_i - (Int32)op2_i;
op1_op2_r = (Int32)op1_r - (Int32)op2_r;
op1_op2_i16 = (Int16)(op1_op2_i >> 1);
op1_op2_r16 = (Int16)(op1_op2_r >> 1);
cplx_prod = (((Int32)op1_op2_r & 0x0000FFFF)<< 16);
cplx_prod = cplx_prod | ((Int32)op1_op2_i & 0x0000FFFF);
return cplx_prod;
}
Where can I find source code of
CPLX_Mul(twiddle[k], data_odd[k]).
CPLX_Add(data_even[k], twiddle_times_data_odd, SCALE_FLAG);
CPLX_Subtract(data_even[k], twiddle_times_data_odd, SCALE_FLAG)
www.ti.com.cn/.../spruh87h.pdf