Part Number: J7200XSOMXEVM
Is it possible to add a fast storage such as SSD drive using the PCIe interface on the J200 evm board? If so what would be the expected through put.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: J7200XSOMXEVM
Is it possible to add a fast storage such as SSD drive using the PCIe interface on the J200 evm board? If so what would be the expected through put.
Hi David,
Can you see the testing done here for an SSD using PCIe. The test was for j721e, but I believe that it would be the same for j7200 as well.
Regards,
Tanmay