I have for same sensor(0X03F10) connect to one soc.
Limited by sensor and structure,one of them needs to be flipped 180°,I need to mirror and filp sensor .
thus,the pattern will change(BGGR to RGGB).In order to patch sensor's bayer,I need to change SOC's pattern from "CFA+AWDR" plugs in.
but when i changge SOC's pattern,the sharpness and color of the picture have changed
The bottom image was taken when I didn't change anything

The bottom image was taken when I change Bayer pattern(BGGR-->RGGB)
-
quesion:
- 1.when i changge bayer pattern ,The hue changed from warm to cool.If R/G and B/G are inberting?Whether I need to correct the white balance
- 2.tivx_aewb_config_t-->sensor_img_phase is Image Format ,Modifying this image doesn't change anything,why.