Other Parts Discussed in Thread: TMS320DM648
Does the TMS320C6655CZH and TMS320DM648 chip have a unique ID?
Is it possible to achieve unique ID through mac address?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does the TMS320C6655CZH and TMS320DM648 chip have a unique ID?
Is it possible to achieve unique ID through mac address?
Sun,
Does the TMS320C6655CZH and TMS320DM648 chip have a unique ID?
No. There is no UID for these chips.
Is it possible to achieve unique ID through mac address?
No.
Regards
Shankari G
read Chip ID from C6678 multicore DSP - Processors forum - Processors - TI E2E support forums
Above links says that the mac addr is unique for each device.
Are these two chips different?
Isn't the mac in these two chips unique?Sun,
Yes, I think you can use the MAC ID - 0x02620110 for C6657/C6655.
I got the value of MAC ID - 0x02620110 as "300A40D3 " ---- In C6657
and "C2B94312 " ---- In C6678. It seems to be unique for the SOC.
--
I do not have TMS320DM648 with me. If you have, do check the appropriate address of the MAC-ID and get the value.
--
For C6657:-------- > IN CCS using Memory browser window

c6655/C6657 - Data sheet -MACID - address:-

Regards
Shankari G