Hello Ethernet Experts,
we have a AM3359 based device, which uses both CPSW Ethernet ports and is operating in swtich-mode. Port 1 is connected to the network, port 2 is connected to a fieldbus processor. Because the DHCP feature of the fieldbus device isn't fully functional, we are looking for a workaround. Is it possible, to receive DHCP Ethernet packages on the A8 host (port 0), which are addressed to the fielbus device? Let's say the host has 192.168.0.8 and the fieldbus device 192.168.0.15. Is it possible to manipulate the ALE, to receive the port 2 dedicated packages on port 0 as well? Some kind of hub mode?
Thanks in advance,
Stephan