Part Number: TDA4VH-Q1
Hi,
I was not able to find in the TRM (SPRUJ52B – JUNE 2022 – REVISED NOVEMBER 2022) if it was MDIO0 or MDIO1 in the MAIN domain that was connected to the internal 9 port Ethernet switch. Could you clarify ?
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VH-Q1
Hi,
I was not able to find in the TRM (SPRUJ52B – JUNE 2022 – REVISED NOVEMBER 2022) if it was MDIO0 or MDIO1 in the MAIN domain that was connected to the internal 9 port Ethernet switch. Could you clarify ?
Best regards
I'm checking on this and will get back to you.
Hi,
Sorry for the delayed response.
if it was MDIO0 or MDIO1 in the MAIN domain that was connected to the internal 9 port Ethernet switch. Could you clarify ?
We can use how ever we want but, this is possible in Linux side by mapping correspond MDIO pins in device tree.
Whereas in case of RTOS application (Ethernet Firmware) mapping as MDIO0 to CPSW2G and MDIO1 to CPSW9G.
We recommend to use as how RTOS application is configured even in Linux side as well.
Best Regards,
Sudheer