Other Parts Discussed in Thread: SN65HVS882, AM3359, TPIC2810, PCA9536, TPS65910
Hii Sir,
I am trying to build dts file for SPI flash Memory(W25Q64) through AM335x Processor but I am getting like this "recipe for target 'arch/arm/dts/am335x-icev1.dtb' failed".
And Here I have added my dts file for spi0 (Using linux kernel version:-4.15.0 and SDK version:-ti-processor-sdk-linux-am335x-evm-05.01.00.11-Linux-x86-Install)
spi0_pins_default: spi0_pins_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x950, PIN_INPUT_PULLUP | MUX_MODE0) /* (A17) spi0_sclk.spi0_sclk */
AM33XX_IOPAD(0x954, PIN_INPUT_PULLUP | MUX_MODE0) /* (B17) spi0_d0.spi0_d0 */
AM33XX_IOPAD(0x958, PIN_INPUT_PULLUP | MUX_MODE0) /* (B16) spi0_d1.spi0_d1 */
AM33XX_IOPAD(0x95c, PIN_INPUT_PULLUP | MUX_MODE0) /* (A16) spi0_cs0.spi0_cs0 */
AM33XX_IOPAD(0x960, PIN_INPUT_PULLUP | MUX_MODE0) /* (C15) spi0_cs1.spi0_cs1 */
AM33XX_IOPAD(0x9a0, PIN_INPUT_PULLUP | MUX_MODE7) /*(B12) mcasp0_aclkr.gpio3[18] */
>;
};
------------------------------------------------------------------------------------------------------------------------------------
&spi0 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&spi0_pins_default>;
sn65hvs882@1 {
compatible = "pisosr-gpio";
gpio-controller;
#gpio-cells = <2>;
load-gpios = <&gpio3 18 GPIO_ACTIVE_LOW>;
reg = <1>;
spi-max-frequency = <1000000>;
spi-cpol;
};
spi_nor: flash@0 {
#address-cells = <1>;
#size-cells = <1>;
/*compatible = "linux,spidev"; */
compatible = "winbond,w25q64","jedec,spi-nor";
spi-max-frequency = <20000000>; /* 20 mhz */
m25p,fast-read;
reg = <0>;
/*partition@0 {
label = "u-boot-spl";
reg = <0x0 0x80000>;
read-only;
};
partition@1 {
label = "u-boot";
reg = <0x80000 0x100000>;
read-only;
};
partition@2 {
label = "u-boot-env";
reg = <0x180000 0x20000>;
read-only;
};
partition@3 {
label = "misc";
reg = <0x1A0000 0x660000>;
};*/
};
};
Regards
Niraj kumar