Hi, dear technical support team, I've been having the following issue every time when I was trying to connect to TMS320C6713B-DSP:
TMS320C671X: Trouble Halting Target CPU: (Error -2130 @ 0x0) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.10.0.00080)
TMS320C671X: Trouble Halting Target CPU: (Error -1060 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.10.0.00080)
The debugger is able to enter into debug-mode and run the code until line 874, as I marked in the blue circle. However, after that, it shows the error "Unable to access device memory" and then it shows the second error. I wonder if anything is set up incorrectly in my device memory. Above you can see my memory setup and the board configuration setup. I've also attached the target configuration setup.
I've been having the same issue over three years on my DSP. Usually, the problem went away automatically after one or two days passive wait. I am not sure what could be going wrong here. Could you double check on my setups that I uploaded and see if there is any obvious mistake? I appreciate your help!
Best,
Decheng