Other Parts Discussed in Thread: SYSCONFIG, TCAN1044V
Hi expert,
Have we measure the waveform from LP-AM263x MCAN1. We got report that the signals doesn't look correct.
We tested MCAN1 on CC board, so MCAN1 module should be no problem.
However, the signal emit from LP-AM263x is wrong. Please refer to capture. We measure the TX signal from J7-64 pin on LP-AM263x.
Basically, we import loopback demo from SDK8.5. Change from MCAN0 to MCAN1. Enable MUX and SEL to route MCAN1_TX, MCAN1_RX to J7 header. And change loopback mode from internal loopback to external loopback so we can get signal on TX pin. Loopback test pass but waveform is wrong. the baud rate is set to 1Mbps/5Mbps.
1. From the measurement, we send 10 64bytes CAN-FD frame, we only got 10 pulses on TX pin. The signal low level can only reach around 1V. Waveform also miss the detail of data.
2. If we connect to external CAN transceiver like TCAN1042/1462EVM , by using 5V and 3.3C on LP-AM263x, we get no signal on TX by the same test software.
3. If we use external power to supply TCAN transceiver VCC and VIO, we can get something on TX and CAN-H, CAN-L. However, the frequency is wrong, TX signal only show 5.5KHZ only.
Question,
1. Is there any limitation regarding LP-AM263x 5V and 3.3V supply? What is the max current it can support?
2. It look like MUX can not drive signal correctly. Can you please check?
Regards
Andre