Hello all,
On the core R5, how can I read the voltage of the core, or the temperature, or the clock speed?
I do not care on reading the data from the Linux, I need to wirte some code and read one of the above on my core.
Is there a direct register to read the voltage?
I read that one can load all kinds of binaries, and it will read, but I would like to use simple code.
Br, Mircea