Hello TI Team,
According to Datasheet Table 5-10. Maximum Current Ratings at AM335x Power Terminals, the current consumption at 3.3V is shown below.
Voltage | SUPPLY NAME | MAX | UNIT |
3.3V | VDDA3P3V_USB0 | 40 | mA |
VDDA3P3V_USB1 | 40 | mA | |
VDDSHV1 | 50 | mA | |
VDDSHV3 | 50 | mA | |
VDDSHV5 | 50 | mA | |
VDDSHV6 | 100 | mA | |
VDDSHV2 | 50 | mA | |
VDDSHV4 | 50 | mA | |
Total | 430 | mA |
I am trying to design a 3.3V supply with a 300mA LDO, could this be a problem?
The IO pins will not be connected to the maximum.
Best Regards,
Kim