我们参考AM437X_INDUSTRIAL_EVM_3K0008_REV1_4A 和AM437X_GP_EVM_3K0006_REV1_4A设计了自己的OP50_Mainboard_AM437x板子。sd卡tisdk-default-image-am437x-evm.wic在买的开发板运行正常。但是在我们的OP50_Mainboard_AM437x板子调试串口没有任何消息输出。是不是tisdk-default-image-am437x-evm.wic带的程序需要修改?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们参考AM437X_INDUSTRIAL_EVM_3K0008_REV1_4A 和AM437X_GP_EVM_3K0006_REV1_4A设计了自己的OP50_Mainboard_AM437x板子。sd卡tisdk-default-image-am437x-evm.wic在买的开发板运行正常。但是在我们的OP50_Mainboard_AM437x板子调试串口没有任何消息输出。是不是tisdk-default-image-am437x-evm.wic带的程序需要修改?
We designed our OP50_Mainboard_AM437x board with reference to AM437X_INDUSTRIAL_EVM_3K0008_REV1_4A and AM437X_GP_EVM_3K0006_REV1_4A. sd card tisdk-default-image-am437x-evm.wic runs normally on the purchased development board. But there is no message output in our OP50_Mainboard_AM437x board debugging serial port. Does the tisdk-default-image-am437x-evm.wic tape need to be modified?
Thanks, tingshan.qin qin. I have assigned the query to our subject matter expert.
Hi,
Does the tisdk-default-image-am437x-evm.wic tape need to be modified?
Yes typically the U-Boot and kernel should be modified and re-configured to work with the new board.
What I want to know is whether debugging information is output before ddr initialization. Because we changed the ddr chip, the ddr may not work properly. Without any debugging information output, there is no way to determine what the problem is
Thanks!