Part Number: SK-AM64
Hi ,
Is it possible to load multiple cores in skam64 at the same time , or to load one arm core from the other arm core like we can do with the R5F and PRU........for example if I consider R5F0 as my main core , and another R5F1 as my remote core so is there a way to load the remote core from the main core , instead of loading it manually ? my use case is I have multiple things to process and for each parameter I want to use a different core for computation. I was checking the example code given in the SDK for IPC notify echo , there it was mentioned that for a multicore program all the executables need to be loaded and run , can this loading be done from a single core or in other words , is there a way to flash multiple SOC initialization binaries at once ?
Regards,
Shruti Gupta