This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TDA4VM: TDA4VL : Can you list out the difference of features supported in SDK's for CDD IPC and PDK IPC ?

Part Number: TDA4VM


Hello,

Can you list out the difference of supported features in CDD IPC and PDK IPC based on SDK versions ?

Regards

Tarun Mukesh

  • Yes, Please find the table below

    TDA4VM-IPC

    SDK8.6 SDK8.4 SDK8.2
    PDK CDD PDK CDD PDK CDD
    Other cores Communication with A72 enabled Yes Yes Yes No Yes No
    call back mechanism No Yes No Yes No Yes
    Major Dependency on PDK Layer Yes No Yes No Yes Yes
    End point selection Dynamic Static (From configurator) Dynamic Static (From configurator) Dynamic Static (From configurator)
    CTRL Endpoint(53) fixed  Yes Yes Yes Yes Yes Yes
    Example of MCU2_1 with A72   Yes Yes Yes No Yes No
    Example of MCU1_0 with A72 Yes No(Present in SDK 9.0) Yes No Yes No

    TDA4VL-IPC

    SDK8.6 SDK8.4 SDK8.2
    PDK CDD PDK CDD PDK CDD
    Other cores Communication with A72 enabled Yes No(Present in SDK 9.0) Yes No Yes No
    call back mechanism No Yes No Yes No Yes
    Major Dependency on PDK Layer Yes No Yes No Yes Yes
    End point selection Dynamic Static (From configurator) Dynamic Static (From configurator) Dynamic Static (From configurator)
    CTRL Endpoint(53) fixed  Yes Yes Yes Yes Yes Yes
    Example of MCU2_1 with A72   Yes No(Upcoming in later SDK) Yes No Yes No
    Example of MCU1_0 with A72 Yes No(Upcoming in later SDK) Yes No Yes No

    Regards

    Tarun Mukesh