Other Parts Discussed in Thread: DRA821
Hi,
Below some questions about difficulties in understanding eye diagram pictures.
I am currently using the Eye_Monitor_tool that comes with the "diag/serdes_diag" package in the pdk_k2hk_4_0_13.
The signal of interest is a 10G entering lane 1 (actually 10.3125 Gb/s)
The typical eye generated by the "EyeDiagramViewer" tool (published in the same package) (with parameters : sensitivity 0.005 ; voltage default 2mV/tap ; Time default 2ps/tap ; Tap width 7 pixels) /
is the following
Here are my questions :
- Can you explain how to calibrate the horizontal axis ? Apparently the axis graduations are not expressed in ps since the eye UI should be more about 97ps than 38 ps that the picture shows;
- Why only 1 eye over 2 seems to be opened (central dark blue area around side the mask) while the other is filled in with light blue scratches ? Can this be due to poor signal integrity , or is it inherent to the tool ?
- in the SPRUHO3a document we can see (lane register @2C) that the Eye fine offset control x-direction is a 7 bit word coding 1/2 UI therefore leading to 1/256 UI per horizontal tap, that is 0.37 ps/tap. Is this correct ?
- The same register includes a 2 bits word in steps of 1/2 UI which therefore creates a possible offset of 3*1/2 UI + 128*1/256 UI = 2 UI. If correct how can we see 4 UI in the above picture ?
- I guess that the EyeDiagramViewer" tool parameters should match the physical characteristics of the 66AK2H14.
- Is the 2mV/tap an adequat setup for 66AK2H14 ?
- Is the 2ps/tap an adequat setup for 66AK2H14 ? note that only integer values are permitted.
Thank you for your help
With best regards,
Bruno