Sorry for not responding to the previous question in a timely manner. We got busy with something else. Back to this now,.
We do enable both PRUs but i think we are only using one. For sure planning to use both in the future.
Repeating text from previous post below.
Hi.
We seem to have the exact same problem as
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1016508/am5708-a15-dsp1-hangs-if-try-to-access-any-register-of-iep-of-pru-icss1-omap_l3_noc-44000000-ocp-l3-application-error-target-5-mod-1-unclearable
When doing HW reset (power cycle) and performing a read or write to e.g. (icssEmacBaseAddressHandle->prussIepRegs + CSL_ICSSIEP_GLOBAL_CFG_REG), or any reg in prussIepRegs, A15 hangs.
This does not happen on soft reset.
However, this issue only occurs in about 1 in 20 boards.
Did you find a solution in the above case.
Thanks for you continuous support,
Anders.