Hi
I can't get AM335x Power Estimation Tool, and AM335x PET Input Spreadsheet from TI.com
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I can't get AM335x Power Estimation Tool, and AM335x PET Input Spreadsheet from TI.com
Hi Liang,
Please see the link below. Remember to select "View all" to expand the drop down. The tool is an excel spreadsheet that needs users to input values and information, and then upload the spreadsheet in the "Step 2" portion of the link below. Within the hour you should receive an email with the PET estimated results.
https://www.ti.com/tool/POWEREST
Regards,
Colin
Hi Colin
When select Cortex A8 NEON 30%, Cortex A8 0%. PET report show Cortex A8 only. Is there any wrong about setting?
Hi Liang,
I am not sure I understand the question - are you setting the A8 to 0% or 30%?
In this case Cortex-NEON is the Cortex A8, in case that is causing confusion.
Regards,
Colin
Hi Colin
are you setting the A8 to 0% or 30%?
RE:Yes
Junt one of them I should select, Cortex A8 or Cortex-NEON. I know that. Thanks.