Part Number: SK-AM64
Is there a Linux command to enable the load switches for VCC3V3_RPI and VCC5V0_RPI on the AM64x Starter Kit board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Bob,
Our subject matter expert is out right now, but I do not think they are exposed in a manner that is easily accessible by default under linux. I'll let Bin comment on this though.
Regards,
Randolph
Hi Bob,
If you use SDK 8.x (which kernel has GPIO sysfs enabled), you can follow the instruction below.
If you use SDK9.0 (which kernel has GPIO sysfs disabled), you would have use gpioinfo and gpioset commands.