Hello Support team.
I tried to make according to the below doc at SK_AM62A_LP.
software-dl.ti.com/.../Top_Level_Makefile.html
Downloaded file is “ti-processor-sdk-linux-edgeai-am62axx-evm-09_00_00_08-Linux-x86-Install.bin”.
Then installed it into Ubuntu 22.04(LTS)
I could successful “make” command.
Also I could successful “make u-boot”
But I got the failure “make install”.
Error Message is the below.
> ================================
> Installing cryptodev-linux
> ================================
> The extracted target filesystem directory doesn't exist.
> Please run setup.sh in the SDK's root directory and then try again.
> make: *** [makerules/Makefile_cryptodev:17: cryptodev_install] Error 1
Of course, I conducted “setup.sh”.
Then I checked the cause of this error. It seems to not define “ROOTFS_PART”.
And this ROOTFS_PART has been defined in Rules.make the below
#root of the target file system for installing applications
ROOTFS_PART?=__ROOTFS_PART__
I would like to know how define __ROOTFS_PART__
I need to set it manually ?
Best Regards
KORO