This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM62A7-Q1: Internal pull configuration registers for MCU_I2C0 and WKUP_I2C0

Expert 7030 points
Part Number: AM62A7-Q1
Other Parts Discussed in Thread: AM62P

Hello Experts,

In the TRM, there is following description

>These bits do not apply to "I2C OD FS" buffer types as these IOs do not have internal pull registers.
>The MCU_I2C0 and WKUP_I2C0 IOs are a special IIC Open Drain Cell I2C_OD_FS.

- What is "FS"?
- Will only the two I2C have the internal pull setting disabled while the other I2C have the internal setting enabled?

Best regards,
Ken