Part Number: TMS320C6713B
Hello,
TMS32C6713BGDPA200 DSP is used as DSP in some of the cards. This DSP stores boot code and some of the system parameters on EMIF flash (INTEL TE28F320C3TD90). Some of erroreneous DSP cards, at the start up (boot), some of the system parameters is read false and after some time later (I guess 730ms) system parameters starts to be read true. I checked the writings on the DSP. All of the errorenous cards have the same DSP symbolizations which is C20-9AC04HW . I am not sure the problem's source is C20-9AC04HW but it is suspicious. So, Is C20-9AC04HW marked DSP different than others when we consider data storage, addressing, boot or etc ? Do you have any experiance ?
Thank you