This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J784S4: Dual eDP display enable in TDA4H SDK version 08.06.01.03

Part Number: PROCESSOR-SDK-J784S4
Other Parts Discussed in Thread: TDA4VH, TDA4VM

Hello TI,

Is there any demo or guideline for enabling second eDP display (port1) in TDA4H qnx SDK? 

  Am facing an issue to enable second eDP (port 1) display in TDA4H with SDK version 08_06 in QNX.I am always getting output at eDP port zero only.

I dont have infotainment card connected ie, am using eDP ports (Port 0 and 1). I have connected one eDP display in port 0 and other eDP display in port 1.

I have enabled "ENABLE_DSS_DUAL" and undefined "ENABLE_DSS_SINGLE" in  "vision_apps/platform/j784s4/rtos/common/app_cfg_mcu2_0.h"

I am running "app_single cam" demo. I am always getting display output at port zero irrespective of  changing the pipeid ie, "obj->display_params.pipeid = 1" 

and also changed the display node target as display 2 in "app_single cam" demo app.

    Please help me to resolve this issue.

Thanks and Regards,

Vineeth