Could you tell me how to use the AM62x Power Estimation Tool?
For Operating Performance Point (OPP):
Q1. Set the operating frequency of each of the compute cores and clusters to 0 MHz to disable it?
For example, "GPU Frequency (MHz)" will be set to 0 for devices without GPU.
But "PRU-SS Frequency (MHz)" cannot be set to 0 since 0 cannot be selected from the list.
Q2. Cannot PRU-SS be disabled?
For Processor Core Utilization (%):
The application note "SPRAD31" is described as follows:
"For guidance, 0% is an "off" or "unused" state. 1% is "idle". 100% is maximum utilization (i.e. Dhrystone)."
Q3. Is the maximum utilization (100%) when processing that is forced to load the cores, such as using the dhrystone benchmark test?
Q4. Is the maximum utilization (100%) when CPU utilization keeps 100% on an OS such as Linux?
Q5. What is the worst case utilization (%) when used for control via various IO and interfaces, and for HMI display and control?
System firmware for security management and resource and power management is provided by TI. TI Foundational Security (TIFS) services will run on HSM, and Resource management (RM) and Power management (PM) services will run on R5F.
Q6. What is the HSM utilization (%) when TIFS is running?
Q7. What is the R5F utilization (%) when RM/PM is running?
The utilization of "Security Accelerator" is a static field.
Q8. Does "Security Accelerator" mean "Crypto Accelerators"?
Q9. Why is the utilization of "Security Accelerator" a static field?
For LVCMOS IO and Peripherals:
"off" and "unused" can be selected from the list in "Mode".
Q10. What is the difference between "off" and "unused"?
The application note "SPRAD31" is described as follows:
"Utilization (%): Specifies the utilization as a percentage of activity relative to a full load condition."
Q11. Does the full load condition mean that data is constantly being sent and received?
Q12. For IOs and Peripherals that support full-duplex, is the utilization less than 50% when only sending or receiving?
Q13. When VOUT is used, is the utilization 100%?
Q14. Is "DDR WR %" the percentage of write accesses out of total accesses?
MMC/SD supports UHS–I DDR50, but "ddr_50mbs" cannot be selected from the list.
Q15. Is it an error that "ddr_50mbs" cannot be selected from the list?
Attach the configured PET sheet here: AM62x_Power_Estimation_Tool_Public_1v1_AM6232ASGGHAALWonMCBD.xlsm
Best regards,
Daisuke