Hi,
Is it possible to do voltage scaling with the TPS65219 pmic?
If yes, is there a reference device tree?
I tried following the device tree "k3-am625-beagleplay.dts" but without success.
I can only permanently set the core frequency to minimum or maximum (0,75/0,85 V), but this does not happen dynamically.
In the opp-table I don't see the thresholds "opp-microvolt", it is normal?
I'm using the new SDK 09.00.00.03 (17 Jul 2023) with kernel 6.1.33.
BR
Domenico Acri