This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: The crystal resonator connected to AM3352 is experiencing abnormal oscillation.

Part Number: AM3352

Hi,

Q1.
When we asked a crystal oscillator manufacturer to match a custom board, we were told that the optimal load capacitance on the board would be 27p to 30pF.

According to the data sheet, the maximum load capacitance is 24pF. The capacitance value of 27pF exceeds the maximum value in the data sheet, but is it possible that abnormal oscillation will occur due to this?

Q2.
Regarding the possibility of abnormal oscillation occurring due to factors other than Q1, I would like to know if there are any possible causes for AM3352.

Thanks,

Conor