This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2SX: MMCAS-RF-EVM and MMCAS-DSP-EVM download FPGA issue

Part Number: TDA2SX


Hi Team,

Download on the diamond programr software using the HW-USBN-2B downloader.

1) The normal download can be done using the SSPI SRAM, as shown in the following figure:

2) Error reported using SPI flash download as shown in the following figure: 

Question A: As shown in 1), it can be downloaded so it can be confirmed this is not a downloader and wiring issue. When download it using the configuration below it will report error, what might be the possible cause? 

B. The customer downloads the FPGA firmware to verify it since their team made a custom board based on the MMCAS-DSP-EVM design files and needs to verify that the firmware is available.

Did TI's FPGA firmware download into nor flash on the FPGA chip via the download method in 2), enabling a one-time download? 

Could you help check this case? Thanks.

Best Regards,

Cherry

  • Please refer to Ch 2.3.2.2 in PROCESSOR_SDK_VISION_03_08_00_00/vision_sdk/docs/Radar/ProcessorSDKRadar_UserGuide.pdf.

    The configuration shown in the guide is what is supported. We don't support any change or FPGA usage on custom board.

    Customer will have to contact FPGA vendor for support.