We are opting to not use the ADC module for ADC conversion. Per the TRM document SPRUIM2G section 12.1.1.4.2.2 we want to set GPI_MODE_EN = 1.
Can these 1.8V logic level inputs we used either as interrupts to the A53 or R5 cores --
OR can these be used as general-purpose inputs to the A53 or R5 cores?