Part Number: 66AK2G12
Other Parts Discussed in Thread: EVMK2GX,
My EVMK2GX board uses MT41K512M8DA-107 (DDR3L) parts, which is speed grade 1866.
The spreadsheet will only let you choose 800, 1066, 1333 or 1600, and it is password protected, and won't allow adding an additional choice.
Our custom hardware we plan to use MT41K512M16VRP-107 DDR parts, (also speed grade 1866) and I'd like to check my understanding of the DDR initialization.
The supplied gel file seems to work on the EVM, and the register values used match the example values in SPRABX7.pdf, so I suspect at some time, someone figured out how to initialize this part.
But I don't seem to be able to enter values from the DDR3L datasheet into the spreadsheet, and get the register values used in the .gel file (or the example in sprabx8.pdf).