I am reviewing bug reports against the TI C7000 CGT compiler in order to determine their impact on a current project and have come across https://sir.ext.ti.com/jira/browse/EXT_EP-11550
The title of this bug is "Introducing temp variable causes different result to be computed" which sounds like it could be a significant issue, but the description doesn't give very much information. Is it only an issue when using boolean types? Is it only an issue when using the compiler intrinsics mentioned in the code snippets? Is it only an issue when declaring variables within for loops?
Since the priority assigned to the issue is "Not prioritised" do TI even accept that the bug exists?
I would appreciate support in understanding this issue more clearly.
Thanks in advance.