Other Parts Discussed in Thread: AM69, FFTLIB, TDA4VH,
Hi TI experts,
I'd like to evaluate the C7x DSP using the AM69 Eval Board within CCS v12.5. I do not intend to use the C7x as AI Accelerator.
So far, I created a project using C7000 Compiler vTI3.1.1. Since my project requires a fft, I used the fftlib from mcu_plus_sdk_am62ax_09_01_00_39.
I was able to build the project.
Now it is unclear to me what Target Configuration File to use for the AM69 Board (is it J784S4_TDA4VH.ccxml?).
Also do I need a .gel file to get the C71x running or is the A72 responsible to start or boot the DSP. In case of A72 is there an example project how to do so?
Same for C7x in general, is there an example project how to debug using CCS?
Thanks & regards
Kim