This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62X-PET-CALC: The initial position of the weston+Qt Dialog window is random

Part Number: AM62X-PET-CALC

Hello

Has anyone ever encountered the problem of weston starting Qt and Qt popping up a Dialog will show in a random initial position

The problem  is as follows picture: When Dialog is opened, the Dialog appears in a random position. And the main window appears randomly when running the program

Expected: The main window position can be initialized at a fixed position, and the Dialog initial position is in the middle of the main window

Linux version:  Linux version 5.10.168

SDK version:  ti-processor-sdk-linux-rt-am62xx-evm-08.06.00.42

in a random initial postino

Expect::

fixed position

How to solve this problem?

whether the new version has fix the bug?

Thanks!


您好

请问关于weston启动Qt和Qt弹出一个Dialog初始位置会随机的问题有人遇到过吗

现象如下图,打开Dialog的时候,Dialog出现的位置随机。并且运行程序的时候主窗口出现的位置随机

期望现象:主窗口位置可以初始化在固定位置,Dialog初始位置在主窗口中间

系统版本:Linux version 5.10.168

SDK版本:ti-processor-sdk-linux-rt-am62xx-evm-08.06.00.42

请问如何解决该问题,或者说新版本是否已经解决该问题?

感谢!