Other Parts Discussed in Thread: OMAPL138, TPS720, TPS7A11
Hello!
I am working on units with a replacement for a platform built on OMAPL138 SoC. I am having trouble with some units intermittently hang during early startup of Linux. We have changed an LDO from TPS72012DRVT to TPS7A1112PDRVR which is used to supply the RVDD pins on the OMAPL138 (E05, H14, N07) and PLL0_VDDA (L15). The units start correctly from the ROM Bootloader (we start U-boot), but fails when we boot Linux.
I suspect that this is because we configure some hardware during early initialzation of linux (I2c, SPI USB etc.) and I can see a voltage drop of about 18mV 1.252- 1.234. This LDO, and the symptoms of the error, is the only change made from a previous version which leads me to believe that it is the cause of the issue.
So to my questions:
- How sensitive is the OMAPL138 SoC to voltage drops on PLL0_VDDA and the RVDD pins? (it seems to me that we are still well within spec.)
- Are there any internals which might be affected by said voltage drop to cause the described behavior? (see serial log below)
```
Starting kernel ...
Uncompressing Linux... done, booting the kernel
```
If there is missing information, I am happy to get back to you with more details. I am primarily a software engineer.
Best regards,
Patrik Nordvall