This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: ti-processor-sdk-rtos-j7200-evm-08_05_00_11 J7200XSOMXEVM J721EXCPXEVM: toolchain problem

Part Number: DRA821U

hello,

I am encountering issues with building linux PSDK 8.5.

it makes error message as follow.

could you let me know direct download URL with gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi toolchain.

Regards,

ryu

ryu@mocean-System-Product-Name:~/smnt3/ti-processor-sdk-linux-j7200-evm-08_05_00_08/yocto-build/build$ MACHINE=j7200-evm   bitbake -k tisdk-default-image

ERROR: Unable to start bitbake server (None)
ERROR: Server log for this session (/home/ryu/smnt3/ti-processor-sdk-linux-j7200-evm-08_05_00_08/yocto-build/build/bitbake-cookerdaemon.log):
--- Starting bitbake server pid 136282 at 2024-03-13 17:27:46.241721 ---
WARNING: Layer meta-psdkla should set LAYERSERIES_COMPAT_meta-psdkla in its conf/layer.conf file to list the core layer names it is compatible with.
ERROR: Failed to obtain external Arm toolchain version: Execution of '/opt/gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -v' failed: command not found
ERROR: Failed to obtain external Arm toolchain version: Execution of '/opt/gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -v' failed: command not found
ERROR: Error: EXTERNAL_TOOLCHAIN path '/opt/gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi' does not exist