Other Parts Discussed in Thread: AM68A
Hi expert,
I'm using EDGE-AI-STUDIO's Model Composer, but Live Preview doesn't work.
The camera image is displayed, inference (Classification, Detection) is not performed.
Could you please let me know if there are any settings that are missing?
[Environment]
- Model Composer:v1.0.0_20240312
- Processor SDK: AM62A v9.00, v9.01, AM68A v9.01
- USB Camera:Logitech C270n HD WEBCAM
- Using "animal_classification" and "animal_detection", images searched on the web are taken with a camera.
- Training and compilation seem to be going well.
- No change even if I change the model
- As a test, I captured the actual AM62A and AM68A with an EVM camera and prepared my own data set, but there was no change in the results.
[Log]
|tidlinferer0 2.01 52.00 19 8 |,|tidlinferer0 1.84 59.19 16 24 |,|tidlinferer0 1.80 55.92 17 43 |,|tidlinferer0 1.79 58.37 17 59 |,|tidlinferer0 1.75 56.31 17 79 |,|tidlinferer0 1.72 55.00 18 100 |,|tidlinferer0 1.71 54.24 18 120 |,|tidlinferer0 1.70 52.28 19 144 |,|tidlinferer0 1.70 48.94 20 175 |,|tidlinferer0 1.70 46.59 21 206 |,|tidlinferer0 1.70 44.90 22 236 |,|tidlinferer0 1.69 43.55 22 267 |,|tidlinferer0 1.69 42.50 23 298 |,|tidlinferer0 1.69 41.63 24 329 |,|tidlinferer0 1.69 40.91 24 360 |,|tidlinferer0 1.68 40.32 24 391 |,|tidlinferer0 1.68 39.80 25 422 |,|tidlinferer0 1.68 39.36 25 453 |,|tidlinferer0 1.68 38.98 25 484 |,|tidlinferer0 1.68 38.64 25 515 |,|tidlinferer0 1.67 38.34 26 546 |,|tidlinferer0 1.67 38.07 26 577 |,|tidlinferer0 1.67 37.82 26 608 |,|tidlinferer0 1.67 37.60 26 639 |,|tidlinferer0 1.67 37.41 26 669 |,|tidlinferer0 1.68 37.24 26 700 |,|tidlinferer0 1.68 37.07 26 731 |,|tidlinferer0 1.68 36.99 27 747 |,|tidlinferer0 1.68 36.85 27 777 |,|tidlinferer0 1.68 36.71 27 808 |,|tidlinferer0 1.67 36.59 27 839 |,|tidlinferer0 1.67 36.47 27 870 |,|tidlinferer0 1.67 36.37 27 901 |,|tidlinferer0 1.67 36.26 27 932 |,|tidlinferer0 1.67 36.17 27 963 |,|tidlinferer0 1.67 36.08 27 993 |,|tidlinferer0 1.67 36.00 27 1024 |,|tidlinferer0 1.67 35.92 27 1055 |,|tidlinferer0 1.67 35.85 27 1086 |,|tidlinferer0 1.67 35.78 27 1117 |,|tidlinferer0 1.67 35.71 28 1148 |,|tidlinferer0 1.67 35.65 28 1179 |,|tidlinferer0 1.67 35.59 28 1210 |,|tidlinferer0 1.67 35.53 28 1241 |,|tidlinferer0 1.67 35.48 28 1271 |,|tidlinferer0 1.67 35.43 28 1303 |,|tidlinferer0 1.67 35.38 28 1334 |,|tidlinferer0 1.66 35.34 28 1364 |,|tidlinferer0 1.66 35.29 28 1395 |,|tidlinferer0 1.66 35.25 28 1426 |
Best regards,
O.H