Other Parts Discussed in Thread: TDA4VH
Hi all,
I am trying to transfer the files from linux pc to the TDA4VH EVM with QNX RTOS using scp command.
I have configured a static IP in the TDA and added the same IP to the pool in Linux. When I try to give scp from Linux to TDA, it is asking for a password and I am not sure if there is any default password for the TDA. I tried giving no password and still getting permission denied.
SDK used : ti-processor-sdk-qnx_j784s4_09_01_00_06 and
ti-processor-sdk-rtos-j784s4-evm-09_01_00_06
Linux:
This is the EVM: