This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AH-Q1: Transfer files from Linux pc to TDA4VH with QNX RTOS using scp command

Part Number: TDA4AH-Q1
Other Parts Discussed in Thread: TDA4VH

Hi all,

I am trying to transfer the files from linux pc to the TDA4VH EVM with QNX RTOS using scp command.

I have configured a static IP in the TDA and added the same IP to the pool in Linux. When I try to give scp from Linux to TDA, it is asking for a password and I am not sure if there is any default password for the TDA. I tried giving no password and still getting permission denied.

SDK used : ti-processor-sdk-qnx_j784s4_09_01_00_06 and 

ti-processor-sdk-rtos-j784s4-evm-09_01_00_06

Linux:

This is the EVM: