Part Number: J7200XSOMXEVM
Hi J7200 Champ,
we are using J721S2XSOMXEVM & J7200 SOM.
Could you please support USB Port enabling on top of PSDK 9.1 or 9.2 ?
we want enable Two USB 2.0 Port.
Best regards,
Ryu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: J7200XSOMXEVM
Hi J7200 Champ,
we are using J721S2XSOMXEVM & J7200 SOM.
Could you please support USB Port enabling on top of PSDK 9.1 or 9.2 ?
we want enable Two USB 2.0 Port.
Best regards,
Ryu
HI Ryu
Could you please support USB Port enabling on top of PSDK 9.1 or 9.2 ?
There no support for the USB driver in RTOS SDK only Linux SDK has.
If you want to enable the USB2.0 port hub in Linux SDK you can follow the below FAQ.
Regards
Diwakar
Hi Diwakar,
i has already tried applying that patch, but it didn't work.....
Do we need to configure the hardware dip switch settings?
Best regards,
Ryu
HI Ryu
Where you are connecting your USB device to the TYPE A port hub right ?
Have you tried analysing logs ?
Regards
Diwakar
hello Diwakar,
yes, i used 2 usb hub port.
when i checked booting log, i can not find error.
when plug in usb device, there is no kernel message.
regards
ryu
hello Diwakar,
I've confirmed that I applied the patch incorrectly. It's working fine now.
thank you
regards
ryu