Hi, I remember back to 2016, software level calibration is required to obtain optimal DDR parameters in every PCB board. But now I see the tuning websites are gone, and the EMIF tools document was updated in 2019.
I only have one DDR in my design. Based on the document, I do not need to run the software level calibration. I only need to fill in the spreadsheet and get optimal parameters.
Does that mean the parameters I obtained in 2016 is no longer suitable for the new board today? Does the new calibration method only work after a specific version of SDK or uboot ?
Is it recommended to update new parameters to the PCB boards which are mass-produced in 2016?
Thanks
Andy S.