Other Parts Discussed in Thread: DRA829
What is the power consumption range for DRA829V-Q1 subsystem with followings?
- 8GB DDR SDRAM
- 64MB NOR flash
- PCIe Gen3x2 lanes SSD
- 32GB eMMC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the power consumption range for DRA829V-Q1 subsystem with followings?
The primary power consumption in the DRA829 device is in the core IP blocks and in the backplane; the peripherals are typically small-ish contributors.
At 125C, the typical power for an ADAS application will be about 17W. The following table gives a broad range for different junction temperatures.
|
10.5 W – 21.5 W |
Tj = 125°C |
|
8.3 W – 18.2 W |
Tj = 105°C |
|
7.0 W – 16.4 W |
Tj = 85°C |