I have created a separate project in my workspace for SD example code, I followed "CSL_MMCSD_SdCardExample" project properties into my project and included also dependent folder "C55XXCSL_LP". After building the project the following error is shown in the log
Invoking: C5500 Linker
"C:/ti/ccs1270/ccs/tools/compiler/c5500_4.4.1/bin/cl55" -v5505 --memory_model=large -g --define=c5505 --display_error_number --diag_warning=225 --ptrdiff_size=16 -z -m"AudioPlayer.map" --stack_size=0x200 --heap_size=0x400 -i"C:/ti/ccs1270/ccs/tools/compiler/c5500_4.4.1/lib" -i"C:/ti/ccs1270/ccs/tools/compiler/c5500_4.4.1/include" --priority --reread_libs --display_error_number --warn_sections --xml_link_info="AudioPlayer_linkInfo.xml" --rom_model --sys_stacksize=0x200 -o "AudioPlayer.out" "./audioplayer.obj" -l"C:/ti/c55_lp/c55_csl_3.08.01/ccs_v6.x_examples/C55XXCSL_LP" -llibc.a
<Linking>
fatal error #6001: cannot open file
"C:/ti/c55_lp/c55_csl_3.08.01/ccs_v6.x_examples/C55XXCSL_LP": Permission
>> Compilation failure
denied
makefile:135: recipe for target 'AudioPlayer.out' failed
gmake[1]: *** [AudioPlayer.out] Error 1
makefile:131: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****
If it is just a file permission error then how to solve.
Could anyone please help.