I want to check the USB 3.0 rate of 5Gbps only applies to configuring the AM6442 (via the A53 core) as a USB 3 host not as a USB 3 device - please confirm! (Means we are limited to 480Mbps as a device?)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to check the USB 3.0 rate of 5Gbps only applies to configuring the AM6442 (via the A53 core) as a USB 3 host not as a USB 3 device - please confirm! (Means we are limited to 480Mbps as a device?)
Hello Jim Mrowca,
Thank you for the query.
I am assigning the query to the expert.
Regards,
Sreenivasa
Hello Jim Mrowca,
Our USB software expert confirmed that USB3.0 in device mode is not supported, only USB2.0 in device mode is supported.
I have requested our USB expert to additionally add his thoughts to the thread.
Regards,
Sreenivasa
Greetings Kallikuppa:
I would think TI will be trying to get USB4(r) interfaces on future Sitara products.
Having said that, I will question if the present AM6442B*ALV* silicon can get to USB 3.1 10Gbps host & master transfer rates WITHOUT a die rev (i.e. avoid a AM6442C*ALV)?
thanks
Jim
Hello,
USB 3.1 GEN2 (10G) is not currently possible with AM64xx and there is no plan to add support for this.
Thanks DK for the response;
Do we think that even USB 3.1/3.2 or even USB4(r) could be supported in any future Sitara product?
thanks
Jim Mrowca (ex-TIer 1982-1997)