This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J721EXSOMXEVM: Configure the weston.ini to change resolution of display when connected via DP port on J721E EVM board

Part Number: J721EXSOMXEVM


Tool/software:

Hi,

We would like to modify the resolution and the refresh rate when we connect an external display via the DP port of the device. Can someone from the community please point out as to where in weston.ini do we need to make the change so that it works for the display connected via DP port.

Thank you.