This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 UART Serial Flasher flashing issues - Waiting for SFT on the DM36x.. Target: BOOTME



Hello

I am trying to flash the DM365 via UART Serial Flasher, but getting BOOTME  message, why it is not getting further?

Thank you

Kumar

-----------------------------------------------------

TI Serial Flasher Host Program for DM36x

(C) 2009, Texas Instruments, Inc.

Ver. 1.50

-----------------------------------------------------


Platform is Windows.

Flashing NAND with ubl_DM36x_ARM297_DDR243_OSC24_NAND.bin and T:\2011+\TI\DaVinc

i-PSP-SDK-03.21.00.04\DaVinci-PSP-SDK-03.21.00.04\images\kernel\dm36x\uImage.


Attempting to connect to device COM1...

Press any key to end this program at any time.

Waiting for the DM36x...

BOOTME commmand received. Returning ACK and header...

ACK command sent. Waiting for BEGIN command...

Target: BEGIN

BEGIN commmand received. Sending CRC table...

100% [ ]

CRC table sent....


Waiting for DONE...

DONE received. Sending the UBL...

100% [ ]

UBL sent....


DONE received. UBL was accepted.

UBL transmitted successfully.


Waiting for SFT on the DM36x...

Target: BOOTME

Target: BOOTME

Target: BOOTME

.

.

.

.