Tool/software:
Dear All,
i would like to know if it is supported in AM68A PCIe lane swapping?
My current design
Can you swap TX0 lane with TX1 lane? in this case do i need to swap also the RX0 lane with RX1 lane?
Regarding the lane length matching:
DO i need to length match TX0, TX1,TX2 and TX3 lane?
DO i need to length match RX=,RX1,RX2 and RX3 lane?
Best Regards,
d.