Tool/software:
Customer said In the IBIS model, differential signals like DDR DQS P/N are all inverted, please help to confirm, and if it impact simulation result?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Customer said In the IBIS model, differential signals like DDR DQS P/N are all inverted, please help to confirm, and if it impact simulation result?
Hi Tony,
Can the customer please replace lines 1511-1530 within the IBIS model with the following?
AC1 AB2 NA NA NA NA || DDR0_CKP & DDR0_CKN U1 V1 NA NA NA NA || DDR0_DQS0P & DDR0_DQS0N AA1 Y1 NA NA NA NA || DDR0_DQS1P & DDR0_DQS1N AF1 AE1 NA NA NA NA || DDR0_DQS2P & DDR0_DQS2N AJ1 AH1 NA NA NA NA || DDR0_DQS3P & DDR0_DQS3N B10 A11 NA NA NA NA || DDR1_CKP & DDR1_CKN A16 A17 NA NA NA NA || DDR1_DQS0P & DDR1_DQS0N A13 A14 NA NA NA NA || DDR1_DQS1P & DDR1_DQS1N A8 A9 NA NA NA NA || DDR1_DQS2P & DDR1_DQS2N A3 A4 NA NA NA NA || DDR1_DQS3P & DDR1_DQS3N L2 K1 NA NA NA NA || DDR2_CKP & DDR2_CKN T1 R1 NA NA NA NA || DDR2_DQS0P & DDR2_DQS0N N1 M1 NA NA NA NA || DDR2_DQS1P & DDR2_DQS1N H1 G1 NA NA NA NA || DDR2_DQS2P & DDR2_DQS2N E1 D1 NA NA NA NA || DDR2_DQS3P & DDR2_DQS3N A24 B25 NA NA NA NA || DDR3_CKP & DDR3_CKN A18 A19 NA NA NA NA || DDR3_DQS0P & DDR3_DQS0N A21 A22 NA NA NA NA || DDR3_DQS1P & DDR3_DQS1N A26 A27 NA NA NA NA || DDR3_DQS2P & DDR3_DQS2N A29 A30 NA NA NA NA || DDR3_DQS3P & DDR3_DQS3N
This will flip the differential pairs.
Regards,
Mark