This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J721EXSOMXEVM: J721EXSOMXEVM: What conditions should be used to determine whether or not PROXY for UDMA Rx/Tx Channel

Part Number: J721EXSOMXEVM
Other Parts Discussed in Thread: DRA829

Tool/software:

Hello!

We have a questions about RINGACC and PROXY  or J721E DRA829.

What conditions should be used to determine whether or not PROXY should be used when RINGACC is used?

When the Ether driver communicates with a communication load listed, the state of the RIINGACC for COMPLETE used in the transmission completion becomes incorrect.

Popping data from the COMPLETE queue through PROXY has improved the situation, but we do not know why.

We would appreciate your opinion on whether this is the correct response.

SDK file name:
ti-processor-sdk-rtos-j721e-evm-08_05_00_11.tar.gz

Driver directory Name:
ti-processor-sdk-rtos-j721e-evm-08_05_00_11/pdk_jacinto_08_05_00_36/packages/ti/drv/udma