This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62-LP: Boot Performance Capabilities of SK-AM62-LP - Android + FreeRTOS Automotive Head Unit

Part Number: SK-AM62-LP
Other Parts Discussed in Thread: AM62P

Tool/software:

Following are a list of Performance Requirements -

1. Android Cold boot up time - <30Secs from application of Accessory Power

2. FreeRTOS Cold boot up time - <2secs from application of Accessory Power

3. Wake up from STR (Suspend to RAM) < 2Secs from Wake up Event

4. RVC app launch by Android < 5 secs from Vehicle Ignition

5. RVC video latency < 200msecs from launch of RVC app

6. Touch response < 100msecs from on boot complete

7. System Shutdown Time < 10secs from user input to Shutdown

8. CAN Bus Communication Latency < 100ms from System Ready

9. OTA Reliability - 99%

Please help to clarify if these (Whichever is applicable to the SoC) are achievable with the Android Automotive OS (AAOS) and FreeRTOS SDKs provided by TI for SK-AM62-LP.
Also please clarify till when AAOS is supported for security update and bug fixes