Tool/software:
I recently got an evaluation kit from TI, SK-AM62-SIP. I'm trying to get it to boot following the quick start guide.
It is unable to boot. There are no serial logs from the J15 microusb port.
This are the sd images that I used.
- tisdk-default-image-am62xxsip-evm.rootfs.wic.xz — 567794 K
- tisdk-default-image-am62xx-evm.rootfs.wic.xz — 890226 K
I have also tried different versions V10x, V09x, V08x, with no effect.
Following the guide, I have also renamed the tiboot files accordingly. Where the tiboot3-am62x-gp-evm.bin is tiboot3.bin.
Ps. I have also tried without renaming the files.
The closest I got to any serial logging is with the v08x ,tisdk-default-image-am62xx-evm.wic.xz — 351027 K, without renaming the tiboot3.bin.
The pin configuration for the Eval kit is as follows, B0 11000010 01000000 B15
What am i missing?