Other Parts Discussed in Thread: TPS65219
Tool/software:
Dear Expert.
This is a double check.
(1) MPU : AM6254ATCGHAALW (ALW package, T speed grade)
(2) PMIC : TPS6521902 (Support LPDDR)

Q1 : Because of ALW package do not have "VDDA_DDR_PLL0" pin, This power rail is internally connected to VDD_CORE in the ALW package. So we don't care VDDA_DDR_PLL0 pin connection in ALW package, Am I correct?
Q2 : If we use TPS6521902, the VDD_CORE of AM62x is 0.75V only, Am I correct?
Q3 : I found TPS6521908 is also another choice for LPDDR, and VDD_CORE is 0.85V, but its LDO2 is disable. What's kind of user case for TPS6521908?
Many Thanks
Gibbs